FFT and complex mtrix processing capabilities on top NXP S32R/V

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FFT and complex mtrix processing capabilities on top NXP S32R/V

ソリューションへジャンプ
2,700件の閲覧回数
shai_b
Senior Contributor II

Hello Team

I have a customer who developing a radar (based TI chipset) cascading device up to 4 devices (72ch,).

the customer would like to have the following processing capabilities with the required benchmarks.

Please advise what is the best suitable S32R/V SoC accordingly:

process_cap.png

 

 

 

 

 

I was thinking to offer S32R45 which has 4ch. of MIPI-CSI2 with Linear algebra accelerator that could suit their needs, waiting for your kind recommendation?

Thanks in advance

Regards,

Shai

タグ(1)
0 件の賞賛
返信
1 解決策
2,681件の閲覧回数
GaryRK
NXP Employee
NXP Employee

Hello Shai,

S32R45 is indeed the most suitable device for that use-case. From connectivity perspective it is the only one capable of interfacing with 4 MMIC devices since it has 4 * CSI2 interfaces and multiple SPI/I2C/Ethernet. From processing capability perspective it exceeds those expectations comfortably.

Regards,

Gary

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,682件の閲覧回数
GaryRK
NXP Employee
NXP Employee

Hello Shai,

S32R45 is indeed the most suitable device for that use-case. From connectivity perspective it is the only one capable of interfacing with 4 MMIC devices since it has 4 * CSI2 interfaces and multiple SPI/I2C/Ethernet. From processing capability perspective it exceeds those expectations comfortably.

Regards,

Gary

0 件の賞賛
返信
2,670件の閲覧回数
shai_b
Senior Contributor II

Hi @GaryRK ,

Thanks for your comments.

Could you please share with me the MIPI-CSI2 Characterization such as the numbers of lanes per port, the bandwidth of each line?

I really appreciated your assistance, Thanks n advance 

Kind regards,

Shai

0 件の賞賛
返信