Execution code in ram

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Execution code in ram

2,737 Views
markulhu
Contributor II

hi, for my eeprom driver designing, i copyed the code from flash to ram,but jump to code in ram, it cause "HardFault" exception. is there any configuration that must be set manually? 

//static Std_ReturnType Eep_EnEepRam(void)

{

FTFC_FCCOB0 = 0x81; /* SETRAM */
FTFC_FCCOB1 = 0x00; /* FlexRAM available for emulated EEPROM */
FTFC_FSTAT |= 0x80; /* Launch command */
while (FTFC_FSTAT & 0x80) {}
return FTFC_FSTAT == 0? E_OK: E_NOT_OK;

}

//void Eep_Init(void)

{

const uint8* EnEepFun;
uint8* LoadRam = (void*)0x1FFFF000;
uint32 Depart;

Depart = (SIM_FCFG1 & 0xF000) >> 12;


if (Depart == 3 || Depart == 4 || Depart == 8 || Depart == 10 || Depart == 11)
{
EepRamEnabled = TRUE;
return;
}

EnEepFun = (const void*)Eep_EnEepRam;

(void)memcpy(LoadRam, EnEepFun, 20);
if (((Std_ReturnType(*)(void))LoadRam)() == STD_OK)
{
EepRamEnabled = TRUE;
return;
}

}

2 Replies

2,652 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Steven,

You can use code below to place the function into the RAM and after that just use the name of the function to call.

__attribute__ ((section(".code_ram"))) // place the code below into .code_ram section
void YourFunction(void);

Or you can check the S32_SBC[CFSR] register. For more details, please, look at the Cortex-M4 Devices Generic User Guide, chapter 4.3.10: http://infocenter.arm.com/help/topic/com.arm.doc.dui0553b/DUI0553.pdf  

I assume that you use S32K14x.

I hope it helps.

Best regards,

Diana

0 Kudos
Reply

2,652 Views
markulhu
Contributor II

Diana,thanks for your advice!  i have located the reason ,that  because the lowest bit of PC of thumb code must be 1. so i changed LoadRam's value from 0x1FFFF000 to 0x1FFFF001,  it seems running ok.

thank you for your help again!