Example project LPI2C_MASTER

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example project LPI2C_MASTER

Jump to solution
4,179 Views
hajianik
Senior Contributor I

Hi,

For the LPI2C_MASTER project , I don't seem to understand the wiring connection. for S32K44EVB-Q100 the following describes the wiring:

PIN FUNCTION | S32K144EVB-Q100 | S32K144-MB
    ----------------|---------------|--------------
    LPI2C SCL (\b PTA3) |J1-3 - Slave SCL      |J9-30 - Slave SCL
    LPI2C SDA (\b PTA2) |J1-1 - Slave SDA    |J9-29 - Slave SDA
    GND       (\b GND)  |J3-11 - Slave GND    |J6 - Slave GND

So PTA3/PTA2 where are they connected to, don't we need a pull up on SCL(PTA3)?

0 Kudos
Reply
1 Solution
3,790 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

These pins PTA2/PTA3 are connected only to the J1 header.

Pin configuration of this example is set in 2-pin open drain mode (see register MCFGR1) which requires pull-ups. Internal pull-ups are enabled by default (PORTA[PCR]) so you can see the communication on scope. It might work but in general these internal pull-ups are week for I2C communication so you should use external pull-ups.

 

Regards,

Daniel

View solution in original post

0 Kudos
Reply
4 Replies
3,086 Views
peter09
Contributor III

please uplode working example of lpi2c master for s32k144evb bord

0 Kudos
Reply
3,791 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

These pins PTA2/PTA3 are connected only to the J1 header.

Pin configuration of this example is set in 2-pin open drain mode (see register MCFGR1) which requires pull-ups. Internal pull-ups are enabled by default (PORTA[PCR]) so you can see the communication on scope. It might work but in general these internal pull-ups are week for I2C communication so you should use external pull-ups.

 

Regards,

Daniel

0 Kudos
Reply
3,790 Views
hajianik
Senior Contributor I

Thanks for your reply

So there is actually no Slave device, So who is sending ACK and other frames from Slave. Or this is just sending 255 bytes in one shot with one stop at the end without receiving any thing from any slave?

Thanks,

Koorosh Hajiani

0 Kudos
Reply
3,790 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Yes, that's correct. The S32K144 device has only one LPI2C instance. So you need two boards, one as a master and one as a slave, or another I2C device.

Regards,

Daniel