Ethernet in MII mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,140件の閲覧回数
rak14
Contributor III

Hi,

I'm using S32K148 Microcontroller, will it support MII mode with PHY?

What are settings needs to be done to work in MII mode?

Should TX_CLK and RX_CLK configured for 2.5MHz/25MHz?

0 件の賞賛
返信
1 解決策
2,103件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, S32K148 support MII mode.
On MCU side, the ENET module have to be set for MII mode and all needed pins properly initialized.
Thy PHY must be set for MII mode as well, either using bootstrapping options or later by updating PHY registers using SMI interface.
TX_CLK/RX_CLK are inputs on MCU side, a PHY is generating those clock signals.

BR, Petr 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,104件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, S32K148 support MII mode.
On MCU side, the ENET module have to be set for MII mode and all needed pins properly initialized.
Thy PHY must be set for MII mode as well, either using bootstrapping options or later by updating PHY registers using SMI interface.
TX_CLK/RX_CLK are inputs on MCU side, a PHY is generating those clock signals.

BR, Petr 

0 件の賞賛
返信