Error during flash programming,S32K144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error during flash programming,S32K144

6,086 Views
lhz
Contributor I

Dear All,

    I got a problem when I was writing the Bootloader of S32K144,I couldn‘t download my program with the Multilink Universal, the error was:

"Error  during flash programming, Terminating debug session".

I opened the PEMicro debug configuration and select"Emergency Kinetis Recovery using mass erase"in Debugger tab, but it still didn't solve the problem, I meet the problem on two S32K144 board.

Thank you!

  Linghou Zeng

0 Kudos
Reply
2 Replies

5,822 Views
johnny_pe
Contributor III

Hi Linghou,

Your console output shows the following error message:

Error! CRC Command Timed Out

CMD>EM

Command is inactive for this .ARP file.

This can happen if your MCU resets while the algorithm is trying to perform an operation. 

Please send us an email to [email protected] with a summary of your complete hardware and software setup so we can help you troubleshoot this issue.

Regards,
Johnny

PEmicro Support

0 Kudos
Reply

5,823 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Linghou,

Have you tried to load the different project into MCU?

Can you share the linker file?

Also, you can try to look at the registers by "Attach to Running Target" option in the Debug Configuration -> Startup.

Best Regards,

Diana

0 Kudos
Reply