Error during flash programming,S32K144

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error during flash programming,S32K144

3,698 次查看
lhz
Contributor I

Dear All,

    I got a problem when I was writing the Bootloader of S32K144,I couldn‘t download my program with the Multilink Universal, the error was:

"Error  during flash programming, Terminating debug session".

I opened the PEMicro debug configuration and select"Emergency Kinetis Recovery using mass erase"in Debugger tab, but it still didn't solve the problem, I meet the problem on two S32K144 board.

Thank you!

  Linghou Zeng

0 项奖励
回复
2 回复数

3,434 次查看
johnny_pe
Contributor III

Hi Linghou,

Your console output shows the following error message:

Error! CRC Command Timed Out

CMD>EM

Command is inactive for this .ARP file.

This can happen if your MCU resets while the algorithm is trying to perform an operation. 

Please send us an email to technical-info@pemicro.com with a summary of your complete hardware and software setup so we can help you troubleshoot this issue.

Regards,
Johnny

PEmicro Support

0 项奖励
回复

3,435 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Linghou,

Have you tried to load the different project into MCU?

Can you share the linker file?

Also, you can try to look at the registers by "Attach to Running Target" option in the Debug Configuration -> Startup.

Best Regards,

Diana

0 项奖励
回复