Error For Importing a Memory Dump File to FlexNVM EERAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error For Importing a Memory Dump File to FlexNVM EERAM

ソリューションへジャンプ
4,108件の閲覧回数
turgaykale
Contributor III

Hi,

I am using an EEPROM Emulation feature of FlexNVM in S32K148 MCU. I am using S32 Design Studio v3.4 IDE. I have got an error when importing a memory dump file (already exported and saved in srec format) to FlexRAM address starting from 0x1400_0000 to 0x1400_0400 which is a FlexRAM memory range used to emulate EEPROM Emulation feature of FlexNVM. Would you please help to understand the reason behind this type of error? Is it possible to import a memory dump file to FlexRAM (in our case: address from 0x1400_0000 to 0x1400_0400) when using an EEPROM emulation feature of FlexNVM ?

Importing a memory dump file (srec format) via memory browser window:

turgaykale_1-1640348317902.png

Error is:

turgaykale_2-1640348673247.png

Thank you !

 

0 件の賞賛
返信
1 解決策
4,079件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @turgaykale,

When EEERDY = 1, every write (8bit, 16bit or 32bit) to the EEEPROM clears the CCIF flag and the EEPROM must not be written until CCIF is set again.

Please refer to AN11983 Using the S32K1xx EEPROM Functionality

https://www.nxp.com/docs/en/application-note/AN11983.pdf

 

Based on that, I don't think the S32DS can do that.

It should be possible to load the data to SRAM.

 

Regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,080件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @turgaykale,

When EEERDY = 1, every write (8bit, 16bit or 32bit) to the EEEPROM clears the CCIF flag and the EEPROM must not be written until CCIF is set again.

Please refer to AN11983 Using the S32K1xx EEPROM Functionality

https://www.nxp.com/docs/en/application-note/AN11983.pdf

 

Based on that, I don't think the S32DS can do that.

It should be possible to load the data to SRAM.

 

Regards,

Daniel

0 件の賞賛
返信
4,056件の閲覧回数
turgaykale
Contributor III

Thank you Daniel for the comment !

0 件の賞賛
返信