Enable Hysteresis for UART Rx on S32K116

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Enable Hysteresis for UART Rx on S32K116

1,750 次查看
satheesh_mb
Contributor I

Hi,

Can I configure Hysteresis for UART Rx pin. If yes Can I configure to different values?

Thanks,

Satheesh.

0 项奖励
回复
1 回复

1,714 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Satheesh, 

These pins can be configured with an internal pull-up, pull-down, or with neither of these two options. You cannot configure different values for the internal pull-up/pull-down resistor. 

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------- 

0 项奖励
回复