Enable Hysteresis for UART Rx on S32K116

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable Hysteresis for UART Rx on S32K116

1,757 Views
satheesh_mb
Contributor I

Hi,

Can I configure Hysteresis for UART Rx pin. If yes Can I configure to different values?

Thanks,

Satheesh.

0 Kudos
Reply
1 Reply

1,721 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Satheesh, 

These pins can be configured with an internal pull-up, pull-down, or with neither of these two options. You cannot configure different values for the internal pull-up/pull-down resistor. 

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------- 

0 Kudos
Reply