ETM support for S32K342 Micro

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ETM support for S32K342 Micro

1,187件の閲覧回数
siva280386
Contributor I

Hello,

   As per the micro reference manual, we see that ETM module is not available in S32K342 and we have to choose the next version S32K344 micro which is only coming in 176 pin package and 4MB flash. For our application , all the other resources supported by S32K342 is good enough with 100pin package and also from cost side. 

  Is there any specific part number in S32K342 that supports ETM or Is there any 

alternative for the trace feature support on S32K342. We understand the JTAG/SWD debug support is there , but the trace supported by ETM - I and ETM - D are not matched to this.

   please let us know if we are missing anything from spec. We would need the data and code trace features supported during debugging our application. 

Thanks,
Siva 

0 件の賞賛
返信
1 返信

1,166件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am afraid it is not.

This feature is only available with S32K344 and this device is only offered with 172 and 257 pin versions.

0 件の賞賛
返信