Differences of RTD develop package

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Differences of RTD develop package

1,578 Views
Hermit
Contributor I

Hi Team

We would like to start a project on S32K342. However, we used S32K344 to test some demo. We now want to transfer S32K344 to S32K342. Some errors appear. 

The RTD package we use before is "SW32K3_RTD_4.4_1.0.0_DS_updatesite_D2110", There is no S32K342. Then we changed it to "SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204". When we build the project which is successful on S32K344 with "SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204" on S32K342, there are a lot of errors. The name of some value changes and some API disappear.

What can I correct them? Or we can not build the project with 2.0.0

 

0 Kudos
Reply
2 Replies

1,566 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Hermit,

SW32K3_RTD_4.4_1.0.0_DS_updatesite_D2110 does not support S32K342, if you want to use S32K342 please install SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204.

The difference between the S32K344 and S32K342 is not just the size of flash memory and RAM. Search for "S32K342" in S32K3XXRM to see all differences. 

Please create new project for S32K342 with RTD2.0.0, import the .mex file and copy the code manually. 

BTW, you can take a look at Low RTD version project immigrating to higher version

Sorry for the inconvenience we bring you!

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,555 Views
Hermit
Contributor I

HI Robin

Thank you for your response.

Best regards,

Hermit

0 Kudos
Reply