ETM support for S32K342 Micro

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ETM support for S32K342 Micro

1,194 次查看
siva280386
Contributor I

Hello,

   As per the micro reference manual, we see that ETM module is not available in S32K342 and we have to choose the next version S32K344 micro which is only coming in 176 pin package and 4MB flash. For our application , all the other resources supported by S32K342 is good enough with 100pin package and also from cost side. 

  Is there any specific part number in S32K342 that supports ETM or Is there any 

alternative for the trace feature support on S32K342. We understand the JTAG/SWD debug support is there , but the trace supported by ETM - I and ETM - D are not matched to this.

   please let us know if we are missing anything from spec. We would need the data and code trace features supported during debugging our application. 

Thanks,
Siva 

0 项奖励
回复
1 回复

1,173 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am afraid it is not.

This feature is only available with S32K344 and this device is only offered with 172 and 257 pin versions.

0 项奖励
回复