ERM INTERRUPT IN THE VECTOR TABLE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ERM INTERRUPT IN THE VECTOR TABLE

ソリューションへジャンプ
3,831件の閲覧回数
hajianik
Senior Contributor I

Hi,

I can't find  ERM sigle/double bit fault interrupts entery in any of the s32k example projects star up code and yet the IRQ number for these interrupts are listed as 44,45 in the header file.

those numbers are mapped in a reserved irq_handler or other peripheral module irqs.

Will you please shed some lite on this,

Thanks,

Koorosh Hajiani

0 件の賞賛
返信
1 解決策
3,802件の閲覧回数
hajianik
Senior Contributor I

THANKS FOR YOUR RESPONSE

I COULD NOT FIND THIS IN THE REFERENCE MANUAL.

WHAT VERSION OF RM IS THIS?

 

THANKS,

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,810件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is according vector table embedded in the reference manual:

davidtosenovjan_0-1629987510947.png

 

Example code you may find here:

https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K14x-SRAM-ECC-Injection/ta-p/1129181

 

 

 

0 件の賞賛
返信
3,803件の閲覧回数
hajianik
Senior Contributor I

THANKS FOR YOUR RESPONSE

I COULD NOT FIND THIS IN THE REFERENCE MANUAL.

WHAT VERSION OF RM IS THIS?

 

THANKS,

0 件の賞賛
返信
3,787件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信