ENET MII no Rx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ENET MII no Rx

2,762件の閲覧回数
jithin_m
Contributor I

Integrated Vector Ethernet stack for Autosar.

Micro: S32K148

Transceiver: Marvell 88Q1010

Interface between PHY and MAC is MII.

During packet transmission no Rx interrupt on ENET, but Tx interrupt is there.

Checked the MII Rx and RX_DV lines.Seems signals present in these lines when data are transmitting from PHY to MAC.But no interrupt on MAC.Also all statistics register values are zeros for Rx.
Also when trying to send packet from MAC to PHY via Eth_Transmit(), data is transmitting via Tx lines and it is receiving on PHY and received on test PC via Media converter board. ie Tx lines are working.
But for Rx MAC not receiving any frames from PHY.

0 件の賞賛
返信
1 返信

2,680件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hi,

Do you still have the issue? If yes, kindly share with us the ETH and PORT configuration, better in xdm or epc, so we can see if your configuration has something incorrect or not.

0 件の賞賛
返信