ENET MII no Rx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ENET MII no Rx

2,798 Views
jithin_m
Contributor I

Integrated Vector Ethernet stack for Autosar.

Micro: S32K148

Transceiver: Marvell 88Q1010

Interface between PHY and MAC is MII.

During packet transmission no Rx interrupt on ENET, but Tx interrupt is there.

Checked the MII Rx and RX_DV lines.Seems signals present in these lines when data are transmitting from PHY to MAC.But no interrupt on MAC.Also all statistics register values are zeros for Rx.
Also when trying to send packet from MAC to PHY via Eth_Transmit(), data is transmitting via Tx lines and it is receiving on PHY and received on test PC via Media converter board. ie Tx lines are working.
But for Rx MAC not receiving any frames from PHY.

0 Kudos
Reply
1 Reply

2,716 Views
namnguyenviet
NXP Employee
NXP Employee

Hi,

Do you still have the issue? If yes, kindly share with us the ETH and PORT configuration, better in xdm or epc, so we can see if your configuration has something incorrect or not.

0 Kudos
Reply