ECU BUS PRO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ECU BUS PRO

12,490 Views
parksuhun
Contributor I
I am trying to implement a Bootloader.
 

I need to load data from a binary file into the MCU, and I understand that ECU BUS PRO performs this function.

However, in the latest version (currently using ECU BUS PRO 0.8.15), there is no option to attach a binary file.

  1. It seems that this feature was available in older versions. Where can I find and download an older version?
  2. Are there any alternative solutions to achieve this?
0 Kudos
Reply
2 Replies

12,433 Views
frankie-zeng
Contributor I
0 Kudos
Reply

12,467 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @parksuhun,

1. You can go into EcuBus' release tab in github (Releases · ecubus/EcuBus-Pro) where you can find all of the preivous releases.

2. You can also refer to the AN12323: S32K1xx Firmware updates – Application Note, which explains the bootloader and firmware update basics, as well as including a demo where one board sends a FW update through CAN, and the second board is updated.

Best regards,
Julián

0 Kudos
Reply