ECC SRAM Reporting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,639件の閲覧回数
smt87
Contributor II

Hi,

I am using S32K11x MCU for my project. I want to use ECC reporting for safety mechanism, so I want to learn how can i use this safety mechanism and is there any demo code or any application? I would be glad if someone explain to me.

0 件の賞賛
返信
1 解決策
4,625件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@smt87

yes ,you can refer to AN12522

Senlent_0-1656999250588.png

 

元の投稿で解決策を見る

タグ(1)
0 件の賞賛
返信
5 返答(返信)
4,632件の閲覧回数
smt87
Contributor II

Hi,

In S32K11x on-chip RAM can be used in following applications:
• Safety critical applications: SRAM_U can be used, which starts from 2000_0000.

So S32k11xx only has SRAM_U for app, right?

0 件の賞賛
返信
4,635件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
4,488件の閲覧回数
smt87
Contributor II

Hi,

Do you have any idea how i can check this sample function working correctly?

0 件の賞賛
返信
4,630件の閲覧回数
smt87
Contributor II

Hi,

In S32K11x on-chip RAM can be used in following applications:
Safety critical applications: SRAM_U can be used, which starts from 2000_0000.

So S32k11xx only has SRAM_U for app, right?

0 件の賞賛
返信
4,626件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@smt87

yes ,you can refer to AN12522

Senlent_0-1656999250588.png

 

タグ(1)
0 件の賞賛
返信