ECC Flash Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,105件の閲覧回数
rijil_kp
Contributor III

How to generate an interrupt notification upon the report of an ECC flash error,?.

Is there any configurations available in EB Tresos for this?.

0 件の賞賛
返信
1 解決策
4,070件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

You can refer to here: https://community.nxp.com/t5/S32K/S32K-ECC-error/m-p/878734 and here: https://www.nxp.com/docs/en/application-note/AN12522.pdf Basically, the ECC will be reported when the FLS read failed while checking the checksum value.

元の投稿で解決策を見る

3 返答(返信)
4,084件の閲覧回数
rijil_kp
Contributor III

When will the double bit ECC error for Flash is set?. Will it set if there is a checksum fault in flash?.

0 件の賞賛
返信
4,071件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

You can refer to here: https://community.nxp.com/t5/S32K/S32K-ECC-error/m-p/878734 and here: https://www.nxp.com/docs/en/application-note/AN12522.pdf Basically, the ECC will be reported when the FLS read failed while checking the checksum value.

4,096件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello @rijil_kp,

Any single-bit ECC errors are automatically corrected, and any double-bit ECC errors are reflected onto FERSTAT[DFDIF] flag at the read access from Data Flash or Program Flash. This double-bit ECC error is reported by bus fault/hard fault handler. There isn't any configuration for report the ECC flash error in EB Tresos, unfortunately.

Best Regards,

Nam