EB Tresos Error code 60002

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EB Tresos Error code 60002

Jump to solution
6,667 Views
focusdoit
Contributor III

Hi Community,

I met an issue when I verifed the Mcal Configuration on EB, 

focusdoit_0-1709567730296.pngfocusdoit_0-1709567730296.png

On Error log view,

focusdoit_1-1709567800209.pngfocusdoit_1-1709567800209.png

Does anybody have a clue about it?

0 Kudos
Reply
1 Solution
6,583 Views
focusdoit
Contributor III
0 Kudos
Reply
6 Replies
6,642 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @focusdoit,

Is this an example from the RTD package? Could you share your version of the drivers and EB Tresos? 

Best regards,
Julián

0 Kudos
Reply
6,559 Views
focusdoit
Contributor III

I just did a test on RTD SW32K3_S32M27x_RTD_R21-11_4.0.0_HF01.link,

Added Mcu module, verified, got warning 0, error 0, but when I added the DIO module , not configured it, then I try to verify the project, got

focusdoit_0-1711067455241.pngfocusdoit_0-1711067455241.png

Do you know the reason? thanks

0 Kudos
Reply
6,584 Views
focusdoit
Contributor III
Resolved.
0 Kudos
Reply
6,576 Views
wuxianlong
Senior Contributor I

@focusdoit Hi,

How did you solve it, please? I also encountered the same problem when using RTD4.0.0. But since there was no problem with generating the code, I didn't study it carefully

BRs
xianlong

0 Kudos
Reply
6,515 Views
focusdoit
Contributor III
Perhaps it's RTD issue , tested again, ignore the Error log view, just generate the project, then 0 errors 0 warnigns, even the Error log view was clear. FYI. : )
0 Kudos
Reply
6,559 Views
focusdoit
Contributor III
I just did a RTD configuration test in EB,added 2 modules:MCU and DIO, removed the DIO, then 60002 error was gone.
0 Kudos
Reply