EB Tresos Error code 60002

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EB Tresos Error code 60002

ソリューションへジャンプ
6,709件の閲覧回数
focusdoit
Contributor III

Hi Community,

I met an issue when I verifed the Mcal Configuration on EB, 

focusdoit_0-1709567730296.pngfocusdoit_0-1709567730296.png

On Error log view,

focusdoit_1-1709567800209.pngfocusdoit_1-1709567800209.png

Does anybody have a clue about it?

0 件の賞賛
返信
1 解決策
6,625件の閲覧回数
focusdoit
Contributor III
0 件の賞賛
返信
6 返答(返信)
6,684件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @focusdoit,

Is this an example from the RTD package? Could you share your version of the drivers and EB Tresos? 

Best regards,
Julián

0 件の賞賛
返信
6,601件の閲覧回数
focusdoit
Contributor III

I just did a test on RTD SW32K3_S32M27x_RTD_R21-11_4.0.0_HF01.link,

Added Mcu module, verified, got warning 0, error 0, but when I added the DIO module , not configured it, then I try to verify the project, got

focusdoit_0-1711067455241.pngfocusdoit_0-1711067455241.png

Do you know the reason? thanks

0 件の賞賛
返信
6,626件の閲覧回数
focusdoit
Contributor III
Resolved.
0 件の賞賛
返信
6,618件の閲覧回数
wuxianlong
Senior Contributor I

@focusdoit Hi,

How did you solve it, please? I also encountered the same problem when using RTD4.0.0. But since there was no problem with generating the code, I didn't study it carefully

BRs
xianlong

0 件の賞賛
返信
6,557件の閲覧回数
focusdoit
Contributor III
Perhaps it's RTD issue , tested again, ignore the Error log view, just generate the project, then 0 errors 0 warnigns, even the Error log view was clear. FYI. : )
0 件の賞賛
返信
6,601件の閲覧回数
focusdoit
Contributor III
I just did a RTD configuration test in EB,added 2 modules:MCU and DIO, removed the DIO, then 60002 error was gone.
0 件の賞賛
返信