Driver for Pressure sensor NPB8FD4T1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Driver for Pressure sensor NPB8FD4T1

1,653 Views
Shivanand
Contributor II

Hi, I'm using RDk358BMU which has a pressure sensor, i want to integarte into to my project. Is there any external driver implementation 

0 Kudos
Reply
3 Replies

1,625 Views
RafaR
NXP Employee
NXP Employee

Hi Shivanand

The RD-K358BMU works with the S32K358, so I recommend you check out our SW portfolio for this processor and see which one best suits your needs.

RafaR_0-1742501666864.png

 

I hope this information has helped you, please let me know if you need help with anything else.

Have a great day and best of luck.

0 Kudos
Reply

1,615 Views
Shivanand
Contributor II

Hi @RafaR 

Yes, I have installed the packages, but there is no reference to pressure sensor NPB8FD4T1 in the Packages. Can you look into it?

0 Kudos
Reply

1,550 Views
RafaR
NXP Employee
NXP Employee

Hi Shivanand

I have already done a thorough investigation, this is what I concluded and found:

The RD-K358BMU already has the NBP8-9x internally (the NBP8FD4T1 is from this family), so it is not usual that it needs an extra drive, it should already have the necessary software to work correctly, maybe there is a configuration problem I recommend you follow the following link:

https://www.nxp.com/design/design-center/development-boards-and-designs/sensor-developer-resources/s...

I recommend you download: Application Software for the Host MCU connected to the NBP8 – KE15Z FreeMASTER demo

But if you want to use an external sensor different from the internal one, download this: Application Software for the External MCU connected to the NBP9

 

I hope this information has helped you, please let me know if you need help with anything else.

Have a great day and best of luck.

0 Kudos
Reply