Doubt about S32K144_FOTA_Gateway program

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Doubt about S32K144_FOTA_Gateway program

4,878 Views
AparnaSridharan
Contributor II

When I am searching for bootloader program for S32K144 I came across this following code.

While I am trying to debug the S32K144_FOTA_Gateway I got struct in the following line.

while(0 == (CAN0->IFLAG1 >> CAN_TXbuffer_ptr->MB) & 1 ); //Line No:234 in S32K144_FOTA_Gateway>src>FlexCan.C

Also whether following code can be used for can 2.0 instead of using CAN FD?

AparnaSridharan_0-1645618467123.png

 

10 Replies

4,833 Views
aquant
Contributor II

@lukaszadrapa 

We have connected the Vehicle Spy on the CAN Bus to understand the CAN Communication. But we are not getting the data on the CAN bus. It's getting stuck in the FlexCAN0_transmit while loop.

aquant_0-1646211494579.png

 

Could you let us know why it is getting stuck in the while Loop. What might be wrong ?

We are testing this on our custom hardware with the same pinout used in the s32k evek PTE4 & 5 for CAN TX / RX

0 Kudos
Reply

4,824 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

When checking by an oscilloscope - can you see the signal on TX pin and also on CANH and CANL?

Regards,

Lukas

0 Kudos
Reply

4,820 Views
AparnaSridharan
Contributor II

Hi,

We can't observe CANH and CANL signals through oscilloscope. Actually could you please suggest ways to test CAN bus and what are the configurations needed for CAN bus to work.

 

0 Kudos
Reply

4,806 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Checking of TX and CANH-CANL signals is a key point at the beginning. It's necessary to check if the transceiver is up and running. We can test whatever we want but if there's no signal, it's just wasting of time.

Regards,

Lukas

0 Kudos
Reply

4,772 Views
AparnaSridharan
Contributor II

Hi,

The CAN Part is working with our custom hardware when we generate the code using freemaster. But it is not working with the example bootloader gateway code . The difference what we are seeing on this code are the clock initialization API. Could you please help us what is the difference between these API calls.

In Freemaster 

CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,
g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);

In Example Bootloader Gateway Code, we are seeing the clock initialization with this API

SOSC_init_8MHz(); /* Initialize system oscillator for 8 MHz xtal */
SPLL_init_160MHz(); /* Initialize SPLL to 160 MHz with 8 MHz SOSC */
NormalRUNmode_80MHz(); /* Init clocks: 80 MHz sysclk & core, 40 MHz bus, 20 MHz flash */
LMEM->PCCCR = 0x85000001; /* Invalidate cache & enable write buffer, cache */

0 Kudos
Reply

4,716 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

that's SDK code and baremetal code. You need to check in the SDK if you have the same clock settings as in the baremetal code. The SDK configuration is not visible in that piece of code, you need to check this in Processor Expert.

Regards,

Lukas

0 Kudos
Reply

4,708 Views
AparnaSridharan
Contributor II

Hi,

I have attached Clock configuration and PE file of SDK code below. Also I have compared the clock configurations between SDK code and BareMetal code.  I have observe changes in normal run mode frequency. I have changed that configurations for normal run mode but still it get struck at the same while loop

while(0 == ( (CAN0->IFLAG1 >> CAN_TXbuffer_ptr->MB) & 1 )); 

I have attached files for baremetal code  and SDk also. Could please tell what are the changes we need to make.

0 Kudos
Reply

4,853 Views
AparnaSridharan
Contributor II

Yes the second board is connected to CAN. Using this CAN module we have able to receive messages for other projects. But I am not able to transmit message through CAN from second board using this FOTA_gateway program. Still it is getting struct at this following while statement.

while(0 == (CAN0->IFLAG1 >> CAN_TXbuffer_ptr->MB) & 1 ); //Line No:234 in S32K144_FOTA_Gateway>src>FlexCan.C

 

4,849 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Do you use S32K144-EVB? There's in-built CAN transceiver in SBC UJA1169, so the board needs to be supplied by external 12V, not by USB only. Is the SBC still in forced mode? Or did you execute this example which switch it to normal mode?

c:\NXP\S32DS.3.4\S32DS\software\S32SDK_S32K1XX_RTM_4.0.2\examples\S32K144\driver_examples\communication\sbc_uja116x\

If it is in normal mode, the CAN transceiver in SBC needs to be enabled via SPI. Or it's necessary to switch back to forced mode.

I would try to check by an oscilloscope if you can see the CAN signals on TX-RX and CANH-CANL.

Regards,

Lukas

4,862 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Aparna,

is the second board connected via CAN? This is typical behavior - second board is either not connected or there's some wiring issue...

Yes, the code can be updated to use standard CAN.

Regards,

Lukas