Does S32K provide temperature data?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does S32K provide temperature data?

4,805件の閲覧回数
stephandewit1
Contributor II

Does the S32K1xx, specifically the S32K148UAT0VLQR, provide any type of temperature data? Perhaps from an internal analog channel or maybe another source?

I thought I remember seeing something of this sort some time ago but I cannot find anything in the reference manual.

Thanks,

Stephan

0 件の賞賛
返信
7 返答(返信)

3,880件の閲覧回数
slevitov
Contributor I

Hi Victor, could you also share the information on internal temp. measurement with me? Thanks in advance. 

0 件の賞賛
返信

2,833件の閲覧回数
mstroven
Contributor III

I'm just looking for any reference doc that specifies the degrees C / lsb conversion factor for the internal temp reading on S32K1xx

0 件の賞賛
返信

2,820件の閲覧回数
Matthias_LEHMANN
Contributor III
Hi mstroven,
we've previously used the conversion of NXP's application note AN3031, under the assumption that the S32 would follow a similar behaviour. We've only ever used this function for some quick and dirty engineering assessments and have fairly quickly switched to an external temperature sensor. The readings of the internal sensor also showed some glitches, but that might just be due to the fact, that we didn't put much effort into a robust implementation...
Hope this helps
\\// Matthias

2,817件の閲覧回数
mstroven
Contributor III
Thank you much!
0 件の賞賛
返信

4,713件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Stephan,

I just sent you an email to discuss this thread privately. For further information, please reply to the email that you received.

Best regards,

Victor

0 件の賞賛
返信

3,976件の閲覧回数
Matthias_LEHMANN
Contributor III
Hi Victor,
although it's already a bit older, I'm hijacking this thread instead of opening a new topic. So far we've already been using the internal temperature sensor of the S32K142 for development purposes. Going forward, we'd also like to use it in a released product. Can you please also provide me this information that's apparently not supposed to be publicly distributed?

Thank you, Matthias
\\// Matthias
0 件の賞賛
返信

4,694件の閲覧回数
paulsiegel
Contributor I

Hello Victor, 

for which reason is this information secret?

I am desperately searching on how to read internal ADC like Bandgap and Temperature.

thank you

Paul

0 件の賞賛
返信