Disable eMIOS from input pin via TRGMUX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Disable eMIOS from input pin via TRGMUX

1,202 Views
oskarjohansson
Contributor I

Hi, I am trying to disable eMIOS channels from an input pin using the MCAL.
I am using S32K312 with RTD 2.0.0 D2203.

In the Port config the input pin is set to TRGMUX_TRGMUX_IN6 and in Trgmux Logic Group the hardware input is set to TRGMUX_IP_INPUT_SIUL2_IN6 and hardware output to TGMUX_IP_OUTPUT_EMIOS012_ODIS0. So far, so good I think.

Then in Pwm/ Emios Instance the Output Disable Source is greyed out and I cannot find how to activate the setting.

oskarjohansson_0-1676638520920.png

Best regards,

Oskar

0 Kudos
Reply
2 Replies

1,171 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@oskarjohansson

I spent some time researching, and it's the same on my side, and I can't find a place to configure it.

I need to communicate with the IDE team to confirm whether this is a bug,

At present, you can modify it manually,

thanks for your report.

0 Kudos
Reply

1,166 Views
oskarjohansson
Contributor I

Okay! I will do that meanwhile.

Best regards,

Oskar

0 Kudos
Reply