Default frequency of core and system clock in RUN MODE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Default frequency of core and system clock in RUN MODE

811 次查看
KKumar
Contributor II

Hi Friends,

what is the default frequency of core and system clock of s32 microcontroller??

I am unable to the reset value of SCG_RCCR[DIVCORE] which defines core and system clock

KKumar_0-1665987154958.png

Thanks 

Kishore

0 项奖励
回复
1 回复

804 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Kishore,

Please refer to the FOPT value in /* Flash Configuration */ 

Clock Status Register (SCG_CSR) DIVCORE.pngFTFC_FOPT[LPBOOT].pngFlash Configuration FOPT.png

Hope it helps.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复