Debugging while using external power

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Debugging while using external power

跳至解决方案
2,134 次查看
rjmalmeida0
Contributor III

Hi,

I'm using a S32K116 board. Can I debug using USB Open-SDA interface while powering from a 12V external source? I know that I need to change J107 to position 1-2, but I don't know if the USB will short with the externa power.

Thanks in advance.

标签 (1)
0 项奖励
回复
1 解答
2,046 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Rui Almeida, 

Yes, it is possible to debug with the on-board debugger while powering from a 12V external source. As you mentioned, you only need to change the position of J107 to 1-2 and connect the external power source and the USB cable.


Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,047 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Rui Almeida, 

Yes, it is possible to debug with the on-board debugger while powering from a 12V external source. As you mentioned, you only need to change the position of J107 to 1-2 and connect the external power source and the USB cable.


Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复