Debug Error S32 MPC5744P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug Error S32 MPC5744P

1,527 Views
sametaltun_37
Contributor I

Hi

I bought the MPC5744P Dev-Kit. I installed the S32 program. And I have a problem about the Debugging. When I debug the project. I have an error meseges that is below pictures. I think that, The pc doesn't detect the Decv-kit. But I open the device meneger. I see the devkit. How can I solve this problem ?

Thanks.COM.jpgDebug_Error.jpgDebug_Error_2.jpg

0 Kudos
Reply
1 Reply

1,486 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

do you have a board properly powered? For USB power the J13 jumper must be in position 2-3, for external 12V supply then use J13 1-2 jumper setting.

BR, Petr

0 Kudos
Reply