DMA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DMA

2,441件の閲覧回数
Ayaz
Contributor IV

Hi,

I have some questions regarding DMA:

  1. What is Bandwidth Control, and what effect does it have on a DMA transfer?

  2. What is Source/Destination Modulo? Could you provide an example of how to use it?

  3. What are the Source Last Address Adjustments?

  4. Is Source/Destination Signed Offset the number of bytes that need to be offset?

  5. What effect does enabling the Source and Destination Offset provide?

Skærmbillede 2024-11-22 144544.png

0 件の賞賛
返信
5 返答(返信)

2,421件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Ayaz,

1. Throttles the amount of bus bandwidth consumed by the eDMA. Generally, as the eDMA processes the minor loop, it continuously generates read/write sequences until the minor count is exhausted.

2. The Source Address Modulo (SMOD) defines a specific address range, which is the value after the SADDR + SOFF calculation is performed on the original register value. Setting this field makes it easy to implement a circular data queue in which the size of the queue is a power of 2.

For example.

  • Assume a minor loop size = 4 = 4 NBYTES
  • Julin_AragnM_0-1732301226382.png
  • Julin_AragnM_1-1732301226382.png

     

Julin_AragnM_2-1732301226382.png

3. At the completion of the major iteration count, the source last address value can be used to restore the source address to the initial value or adjust the address to reference the next data structure.

4. Yes, that is applied to the current destination address to form the next-state value as each destination write is completed.

5. Please refer to chapter 15.6.2.10 TCD Transfer Size Without Minor Loop Offsets for a continued explanation:

Julin_AragnM_3-1732301226383.png

Also, I have sent you a private message through the community for a DMA training presentation.

Best regards,
Julián

0 件の賞賛
返信

2,197件の閲覧回数
user_244572
Contributor II
Hello Julian,
Can you send me the DMA training presentation as well ?
Thanks,
0 件の賞賛
返信

2,188件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @user_244572,

I have also sent you a private message through community.

Best regards,
Julián

0 件の賞賛
返信

2,045件の閲覧回数
malove
Contributor IV
Hello Jullian.
Can you send me the DMA presentation as well?

Best regards.
0 件の賞賛
返信

2,436件の閲覧回数
Ayaz
Contributor IV
How can I clear the buffer and start refilling it after each major loop in the most efficient way?
0 件の賞賛
返信