Could sector will be divided into blocks?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Could sector will be divided into blocks?

ソリューションへジャンプ
1,645件の閲覧回数
asd046012
Contributor III

Hello  

    I  see datasheet S32K-RM, find that the program flash memory and data flash memory just have divided into sectors. Because I use the MCU S2K116(P-Flash 128KB, D-Flash 32KB). the size of sector for the  P-Flash and D-Flash are 2KB.

    Are there any smaller units under the sector? for example blocks? If I want to operate the D-Flash, The smallest unit of operation is a sector?

    

 

0 件の賞賛
返信
1 解決策
1,633件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @asd046012,

Do you try to manage the memory in smaller sections in run time? In this case, there's a command called Program Phrase that allows to program 8 bytes. For more information, check section 36.5.9.2 Flash commands in the RM.

Best Regards,

Alexis Andalon

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,634件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @asd046012,

Do you try to manage the memory in smaller sections in run time? In this case, there's a command called Program Phrase that allows to program 8 bytes. For more information, check section 36.5.9.2 Flash commands in the RM.

Best Regards,

Alexis Andalon

0 件の賞賛
返信