Cotactor feedack using ADC with SW triggering

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cotactor feedack using ADC with SW triggering

1,175 Views
Joseph_David
Contributor I

hi, I am currently working on contactor feedback through ADC with software triggering but i the ADC is being either in IDLE or BUSY state, Also i am not sure about the complete configuration changes in the adc and related peripherals , due to some configurations i am getting hard fault. although i have added CDD_m3hhb_adc_exernal_access.h/.c file in the build as well as well as the adc related driver files,  if any body has any reference or example code do, help 

0 Kudos
Reply
3 Replies

1,145 Views
_Leo_
NXP TechSupport
NXP TechSupport

Thank you for your interest in our products and for contributing to our community.

Can you tell us which device are you using please?

0 Kudos
Reply

1,130 Views
Joseph_David
Contributor I
S32k358 microcontroller and LiFePO4 battery pack
0 Kudos
Reply

1,120 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi again,

For ADC SW triggering you could refer directly to RTD examples:

_Leo__0-1749757713164.png

On the other hand, there is the following community post witch cover more software and hardware triggering methods:

https://community.nxp.com/t5/S32K-Knowledge-Base/RTD400-LLD-K344-ADC-SW-HW-trigger/ta-p/1966179

I hope this information is helpful.

0 Kudos
Reply