Code running through AHB on S32K3xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code running through AHB on S32K3xx

ソリューションへジャンプ
7,457件の閲覧回数
OliverTian
NXP Employee
NXP Employee

Hi, 

   For code running through AHB on S32K3xx, tested on SCH-47827 and success.

  Steps are as below.

   1. Allocated functions into QuadSPI AHB space.
   2. Program s-recorder of functions in QuadSPI AHB space into QSPI flash on board
   3. Download project which enables AHB reading into S32K3
   4. Run and enjoy the result. 

Enjoy it!

Oliver Tian

 

 

0 件の賞賛
返信
1 解決策
7,452件の閲覧回数
OliverTian
NXP Employee
NXP Employee

Hi

    With the example project of 'Qspi_Ip_Example_S32K344' in S32DS_3.4, some changes were implemented into linker_flash_s32k344.ld and main.c, as attachments.

Enjoy it. 

Oliver Tian

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
7,453件の閲覧回数
OliverTian
NXP Employee
NXP Employee

Hi

    With the example project of 'Qspi_Ip_Example_S32K344' in S32DS_3.4, some changes were implemented into linker_flash_s32k344.ld and main.c, as attachments.

Enjoy it. 

Oliver Tian

0 件の賞賛
返信
7,449件の閲覧回数
OliverTian
NXP Employee
NXP Employee

Hi

   EVB 's resource could be gotten through the link.

https://www.nxp.com/design/development-boards/automotive-development-platforms/s32k-mcu-platforms/s3...

Enjoy it.

Oliver Tian

0 件の賞賛
返信
7,444件の閲覧回数
OliverTian
NXP Employee
NXP Employee

 

Debugging on AHB space

20220728_115506_S32K3_QSPI_AHB_Function_running.gif

0 件の賞賛
返信