Code generation malfunctions in Flexio_Pwm_Ip_Cfg.h

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Code generation malfunctions in Flexio_Pwm_Ip_Cfg.h

跳至解决方案
2,447 次查看
Gwihan
Contributor II

Q.1: Is there anyone having the same problem as below?

"generate/include/Flexio_Pwm_Ip_Cfg.h:54:10: fatal error: Flexio_Pwm_Ip_BOARD_InitPeripherals_PBcfg.h: No such file or directory"

I thought this message means I have done something wrong. But, this problem is easily solved if I correct header include statement manually (to Flexio_Pwm_Ip_PBcfg.h).

Q.2: What is wrong with template file (of Flexio_Pwm_Ip_Cfg.h) or my configuration?

(I have check my c-code. It will run just fine if the wrong include statement is fixed manually.)

Gwihan_1-1716515972322.png

 

Gwihan_0-1716515236808.png

 

0 项奖励
回复
1 解答
2,426 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please try to test whether the latest S32K3 RTD 4.0.0 has fixed this issue.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,427 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please try to test whether the latest S32K3 RTD 4.0.0 has fixed this issue.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
2,322 次查看
Gwihan
Contributor II
Yes, this has fixed the issue.
Though I had to deal with few problems aroused by difference between two versions, it is worth moving onto RTD 4.0.0.
0 项奖励
回复
2,421 次查看
Gwihan
Contributor II
Is any of RTD 4.0.0 supports S32K312_172MQFP?
RTD I got supports s32k312_hdqfp172.
0 项奖励
回复
2,416 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Yes. These two packages are actually the same, only the name was changed from MAXQFP to HDQFP.

0 项奖励
回复