Code generation failed for peripherals

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Code generation failed for peripherals

10,179 次查看
cw20
Contributor II

Hi,

My project is not building because of code generation failure in the peripherals. According to the error message, no function group is selected to be the default initialization function so it will be empty. How do I fix this?

cw20_0-1686061095201.png

 

0 项奖励
回复
9 回复数

10,126 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @cw20 

When you create a new project you need to add the peripheral which you are needed at first.
After you add the related driver, then you can use the peripheral module in the IDE to configure the related module.

A possibility is that lacks the driver because when you create the project, you did not add the related driver.

Please correct me if this is not your case.

 

B.R.

VaneB

0 项奖励
回复

10,068 次查看
cw20
Contributor II

HI @VaneB ,

 

I am specifically having issues with freeRTOS and tcpip - design studio cannot find the components and that may be why code generation for peripherals is failing. I've included the log file.

0 项奖励
回复

10,064 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @cw20 

Do you have installed on S32DS the FreeRTOS and TCPIP packages?

0 项奖励
回复

10,051 次查看
cw20
Contributor II

Hi @VaneB ,

Yes, I do have both packages installed. And, I installed them in order, FreeRTOS first and then Tcpip second

0 项奖励
回复

9,961 次查看
VaneB
NXP TechSupport
NXP TechSupport

This issue could be caused by code generation timeout.

By default, Peripherals Tool has 15 seconds allocated for code generation (which should be more than enough). If code generation scripts do not finish their execution in 15 seconds, the code will not be generated.

The timeout can occur if the machine on which S32CT is running is slow/heavily loaded/code generation scripts are not optimized.

As a workaround for this issue, code generation timeout can be increased by adding the following argument into the s32ds.ini file (default path could be C:\NXP\S32DS.3.4\eclipse\s32ds.ini, it depends on the version of S32DS).

-Dcom.nxp.swtools.codegenscript.timeout = 60000 -> It will increase code generation timeout to 1 minute.

Or you can increase the timeout based on your environment.

Try this workaround and let me know the result.

0 项奖励
回复

6,503 次查看
HoaMaiXuan
NXP Employee
NXP Employee

Hi VaneB. I am trying by CMD to generate code. I have same issue which have error message is "SEVERE: Peripherals: [SDK] Failed to update the code - Code generation failed.". I tried to increase the timeout param but the issue isn't resolved.

0 项奖励
回复

10,100 次查看
cw20
Contributor II

Hi @VaneB,

I have included all the necessary drivers and MCALs, this is what I have: 

cw20_0-1686101686222.png

 

Thanks.

0 项奖励
回复

10,147 次查看
cw20
Contributor II

Update: I've fixed the functional group error but there is still an issue with code generation for peripherals

cw20_0-1686072259345.png

 

0 项奖励
回复

10,135 次查看
cw20
Contributor II

when I build the project, there is also an issue with the tcpip library that is preventing it from building properly

cw20_0-1686076146477.png

 

0 项奖励
回复