Code for CAN message interaction

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code for CAN message interaction

1,286 Views
lohithn
Contributor I
Hello, Does anyone know code for interacting with S32K148EVB controller using CAN messages? Thank you
0 Kudos
Reply
1 Reply

1,276 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Lohith,

You can refer the examples in S32K SDK, please refer the answer in CAN communication on s32k148EVB-Q144

Notice external 12V power adapter is needed.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply