Clock Source for FLEXCAN in S32k146 controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clock Source for FLEXCAN in S32k146 controller

1,141 Views
VarunT
Contributor I

Am using FIRC -48 MHz as clock source for the FLEXCAN is possible for we need external SOSC

VarunT_1-1717498576628.png

here only SOSCDIV2_CLK is mentioned, does that mean we cannot use FIRC for FlexCAN?

0 Kudos
Reply
1 Reply

1,129 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

FlexCAN protocol clock can be selected either to be SOSCDIV2_CLK or SYS_CLK

PetrS_0-1717526978172.png

If SYS_CLK is running from FIRC then PE Clock can be FIRC as well.
However FIRC is not recommended to supply PE clock due to its accuracy. Use rather SOSC or PLL running from SOSC.

BR, Petr

0 Kudos
Reply