Clarification Needed: J1939 Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Clarification Needed: J1939 Configuration

1,258件の閲覧回数
krupan
Contributor II

We are working on a new implementation using S32K118 coupled with an existing Tresos license (EB Tresos 24.0.1) and MCAL(S32K1XX_MCAL_4.3_RTM_1.0.4)

Our project requires to support for J1939 on top of the standard CAN functionality. Could you please clarify whether this setup supports the J1939 protocol natively, or if there are any additional configuration steps, hardware considerations, or license updates needed to enable this feature?

 

 

 

 

0 件の賞賛
返信
3 返答(返信)

1,233件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @krupan

Unfortunately, NXP does not provide J1939 library. SAE J1939 is higher-layer protocol, so you will need to ask third-party companies for the stack, such as:

Best regards,
Julián

 

0 件の賞賛
返信

1,222件の閲覧回数
krupan
Contributor II

Hi @Julián_AragónM 

We understand now that NXP does not provide a J1939 library and a third-party J1939 stack is required.

Can you please confirm whether the CAN MCAL generated via EB Tresos (v24.0.1) with S32K1XX_MCAL (v4.3_RTM_1.0.4) is fully compatible with a third-party J1939 stack “as-is”? Are there any modifications, configurations, or additional layers needed on the CAN driver side to support SAE J1939 on the S32K118 platform?

0 件の賞賛
返信

1,209件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @krupan,

Yes, there should be no problem, as the stack is high level. However, please confirm this with the third-party, as this may not apply to every implementation.

Best regards,
Julián

0 件の賞賛
返信