Chip Was Locked

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Chip Was Locked

4,113 次查看
wutengyouxi555
Contributor II

The chip seems to be locked

wutengyouxi555_0-1687858803754.pngwutengyouxi555_0-1687858803754.png

If i select yes, reflashing will fail.

how can i unlock it ?  

 

标记 (1)
0 项奖励
回复
5 回复数

4,104 次查看
giraffe508
Contributor IV

Hi @wutengyouxi555 

It seems like you have a locked chip and are unable to reflash it. To unlock the chip, you can follow these steps:

  1. First, you need to perform a mass erase to unlock the chip. This can be done using a debugger or a programmer that supports your specific chip.
  2. Connect the debugger/programmer to your chip and open the software associated with the debugger/programmer.
  3. Find the option to perform a mass erase in the software. This might be located under a menu like 'Debug' or 'Erase'.
  4. Perform the mass erase. This will erase all the contents of the chip, including the flash memory and any security settings.
  5. After the mass erase is completed, you should be able to reflash the chip without any issues.

Please note that performing a mass erase will delete all the data on the chip, so make sure to backup any important data before proceeding.

Best Regards,

0 项奖励
回复

4,083 次查看
wutengyouxi555
Contributor II

wutengyouxi555_0-1688117598367.pngwutengyouxi555_0-1688117598367.png

I've tried unlocking with Jlink command but failed。

here is Console log:

wutengyouxi555_1-1688117846131.pngwutengyouxi555_1-1688117846131.png

Then I tried pulling the pin low using the command,also failed。

Console log:

wutengyouxi555_2-1688117873333.pngwutengyouxi555_2-1688117873333.png

I measured the MCU_NRST pin voltage, result is 0.8V.(The board is energized).

Does that mean the MCU is damaged?

 

 

 

0 项奖励
回复

4,071 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @wutengyouxi555 

Please try to read the MDM_AP status and control registers, to verify the MCU status (Unbricking S32K146). 

 

B.R.

VaneB

0 项奖励
回复

4,048 次查看
wutengyouxi555
Contributor II

wutengyouxi555_0-1688180731544.pngwutengyouxi555_0-1688180731544.png

also failed.

So the chip is already damaged?

0 项奖励
回复

3,961 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @wutengyouxi555 

Unfortunately, there is a high probability that this is the case.

If you did not disable your reset pin maybe something can still be done.

For that, I would like to know if MCU_NRST is your RESET_b pin. If yes, the voltage you mention is very low so the MCU can no longer be recovered.

0 项奖励
回复