Can the HSE firmware and the development source code be integrated into a single binary file?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can the HSE firmware and the development source code be integrated into a single binary file?

790 Views
error81
Contributor I

In order to use the S32K310 chip as a sub-MCU, we plan to load the HSE firmware and add our development source code so that it communicates with the main MCU via SPI. We are considering directly flashing the S32K310 chip using a gang programmer without using JTAG or similar methods. However, our research shows that the HSE firmware must be loaded first, and then the development firmware is added. Therefore, we are inquiring whether there is any way during the development phase to integrate the HSE and the development firmware into a single binary firmware. It would be ideal to flash just one firmware image.

Tags (1)
0 Kudos
Reply
1 Reply

765 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

No, it is not possible.

In single step you would need smarter programmer allowing multiple steps or scripts to be executed.

0 Kudos
Reply