Can't use transfer protocol while in an interrupt function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't use transfer protocol while in an interrupt function

747件の閲覧回数
LBLDT
NXP Employee
NXP Employee

Hi,

I'm using a LPIT timer to trigger the reading and writing of data to my ICs through SPI & I2C. Before, that was done in an infinite loop in the main function but as soon as I paste it in the LPIT trigger function I am always reading STATUS_BUSY with the LPSPI_DRV_MasterGetTransferStatus() function. Did you had this problem before ?

void LPIT0_Ch1_ISR(void){
	LPIT_DRV_ClearInterruptFlagTimerChannels(INST_LPIT0, 1<<LPIT0_CHANNEL1);
	uint8_t spi_data_receive[2];
	hall_singleRead(LPSPICOM0, (uint8_t *)(&UART_command_param.sys_param.spi_read_address), (uint8_t *)(&spi_data_receive), 2);
	MAX5215_setOutput(INST_LPI2C0, &UART_command_param);
	ADC_readConversion(INST_LPI2C0, &UART_command_param);
	enableBuck(&UART_command_param);
	UART_command_param.sys_param.spi_read_value[0] = spi_data_receive[0];
	UART_command_param.sys_param.spi_read_value[1] = spi_data_receive[1];
}

void hall_singleRead(uint32_t instance, uint8_t * sendBuffer, uint8_t * receiveBuffer, uint16_t transferByteCount){
	LPSPI_DRV_MasterTransfer(instance, sendBuffer, NULL, transferByteCount);
	while(LPSPI_DRV_MasterGetTransferStatus(instance, NULL)==STATUS_BUSY){};
	LPSPI_DRV_MasterTransfer(instance, NULL, receiveBuffer, transferByteCount);
	while(LPSPI_DRV_MasterGetTransferStatus(instance, NULL)==STATUS_BUSY){};
}
0 件の賞賛
返信
1 返信

704件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

try to increase interrupt priority for LPSPI. 

BR, Petr

0 件の賞賛
返信