Can not written program into board again.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can not written program into board again.

跳至解决方案
1,635 次查看
liufei
Contributor III

Hello NXP Team,

I make a very simple test for  LED ON by S32K146EVB-Q144 board used PortC by MCAL,

it can be run well on the S32DS for S32 Platform only one time,then the project cannot be stopped and the program cannot be written to the board again.

Mcal setting by EB 23.0.0

IDE is S32DS for S32 Platform.

This problem seems to be caused by the wrong setting of the port to I/O,

It should be set to JTAG,right?

This board can not be written anything now,

Could you tell me how to solve it,thanks!

 

Best Regards,

Liu

0 项奖励
回复
1 解答
1,627 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Liu,

Please check the MCAL setting, if these debug pins are reconfigured to GPIO pins.

JTAG pins.pngJTAG pins.png

Please halt the MCU by refer: Can't use PEmicro debugger with S32K118EVB2-Q048

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,628 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Liu,

Please check the MCAL setting, if these debug pins are reconfigured to GPIO pins.

JTAG pins.pngJTAG pins.png

Please halt the MCU by refer: Can't use PEmicro debugger with S32K118EVB2-Q048

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复