Can not creat a project with S32K342

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not creat a project with S32K342

898 Views
Hermit
Contributor I

Hi Team,

I want to creat a new project with S32K342, but I failed. There is no S32K342 chip for me to choose(I attached a screenshot below). 

The version of S32DS is V3.4 and the version of RTD SDK is "SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204". By the way, I can not open the example where S32K342 is used. There is no example for S32K342! I attached it below.

Need I configure the S32DS or add some special packages to make it applicable to S32K342?

0 Kudos
Reply
2 Replies

885 Views
Hermit
Contributor I

Thank you

0 Kudos
Reply

890 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

be sure right development package is installed into S32DS.

PetrS_0-1673948805896.png

I can see S32K342 option when creating new project

PetrS_1-1673948843804.png

There are examples for S32K342 within RTD package

PetrS_2-1673949469782.png

BR, Petr

 

0 Kudos
Reply