Can D-Flash erase FlexRAM emulating EEPROM?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can D-Flash erase FlexRAM emulating EEPROM?

ソリューションへジャンプ
1,731件の閲覧回数
ShaoTianzhi
Contributor II

Hello: 

I partitioned the FlexNVM of S32K146 into 32K EEP Backup + 32KD-Flash, and placed the main function of the BootLoader project in the D-Flash area. Why did it crash when I tried to erase the EEPROM in the BootLoader project?

0 件の賞賛
返信
1 解決策
1,714件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

In case you are erasing data flash, you must execute the code from code flash. Pay attention to paragraph below>

davidtosenovjan_0-1702640272092.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,715件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

In case you are erasing data flash, you must execute the code from code flash. Pay attention to paragraph below>

davidtosenovjan_0-1702640272092.png

 

0 件の賞賛
返信
1,667件の閲覧回数
Gideon
Contributor III

Dear Telechips:

         I have a need to write EEP in D-Flash(BootLoader). It is said that the RAM solution can write EEP. Can you give me an example?

Gideon_0-1703155475742.png

 

0 件の賞賛
返信