CSEc code yields two different UID's?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CSEc code yields two different UID's?

跳至解决方案
7,546 次查看
gearhead1107
Contributor IV

I'm trying to load crypto keys into my S32 using the example project "1_Configure_part_and_Load_keys", but the "GET_UID()" function yields two different results in the example vs my project on the same part (CSE_PRAM->RAMn[11].DATA_32 is different after the operation, so this seems to be an issue with the example)

The UID generated by the example is different only in the last byte - 21120833 vs 21120865 - while the upper 3 integers are identical, as shown in the two screenshots of the debug instances.

Interestingly, the driver function "CSEC_DRV_GetID" yields something totally different than the example.. is the example just incorrect?

I have attached screenshots of 

UID from the NXP example

{14, 1162432521, 909643814, 21120833}

UID from my project running NXP code 

{14, 1162432521, 909643814, 21120865}

UID from the Driver function which returned "STATUS_SUCCESS"

{edit - this output is erroneous due to some pointer incompatibility - it's the same as the above in RAM}

This is a 0N57U based eval board

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
7,344 次查看
gearhead1107
Contributor IV

It looks like the reason the example yields inconsistent results has to do with the fact "UID" is only 15 bytes. 
The example pulls in a full uint32, including the lower 16th byte, while the UID is *only* those upper 15.

If someone from NXP could confirm, it would be appreciated!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
7,344 次查看
tong_zhou
Contributor I

in mpc5777c manual, the UID's 8 lowest significance bits are set 0.

0 项奖励
回复
7,345 次查看
gearhead1107
Contributor IV

It looks like the reason the example yields inconsistent results has to do with the fact "UID" is only 15 bytes. 
The example pulls in a full uint32, including the lower 16th byte, while the UID is *only* those upper 15.

If someone from NXP could confirm, it would be appreciated!

0 项奖励
回复