CSEc Random Number Generator standard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CSEc Random Number Generator standard

Jump to solution
3,202 Views
Gideon
Contributor III

Architecture was S32K146.  According to the AN5401.pdf,  Random Number Generator standard is:

 1.1 CSEc security module features

• True & Pseudo random number generation

Above, we project need the  Random Number Generator standard choose any one of A ,B, or C:

       A The random number shall be generated with a AIS31 Class P2 compliant generator.
       B ・The random number shall be generated with a AIS20 Class K3 compliant generator.
          ・Input value (SEED) shall be generated with random number generator complying with AIS31                  ClassP1 and more.
       C The random number shall be generated with a NIST SP800-90 compliant generator.

So,could you tell me the CSEc‘s random number generator (RNG) standard satisfies A or B or C?

 

 

 

0 Kudos
Reply
1 Solution
3,185 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Gideon 

TRNG meets requirements given by standards SP800-90B and AIS31 (class PTG.2). PRNG is consistent with the requirements of the predefined class DRG.2 in AIS31.
I can share a document with more details but it is available only under NDA. If you want to get the document, please submit a ticket here:
https://support.nxp.com/s/?language=en_US
Regards,
Lukas

View solution in original post

0 Kudos
Reply
1 Reply
3,186 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Gideon 

TRNG meets requirements given by standards SP800-90B and AIS31 (class PTG.2). PRNG is consistent with the requirements of the predefined class DRG.2 in AIS31.
I can share a document with more details but it is available only under NDA. If you want to get the document, please submit a ticket here:
https://support.nxp.com/s/?language=en_US
Regards,
Lukas

0 Kudos
Reply