CSEc Module for storing secure Encrypted keys and secure boot support in S32K144 MCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CSEc Module for storing secure Encrypted keys and secure boot support in S32K144 MCU

3,259件の閲覧回数
mrajanna
Contributor V

I have gone through below document as well the source code but still I need more information.

http://www.nxp.com/docs/en/application-note/AN5401.pdf

I want to know below details:
a. For the first time how secure keys are loaded into Flash. 
b. 512KB Memory split in S32K144. Memory architecture. 
c. How secure boot is implemented.
d. Any presentation or pdf on CSEc module in S32K144.
e. How CAN messages can be authenticated using CSEc module.
f. After purchase of evaluation board, Would I get help to program secure encrypted keys and secure boot.

タグ(1)
0 件の賞賛
返信
1 返信

2,308件の閲覧回数
liulei1
Contributor II

Hello, my problem is the same as yours. Have you solved it?

0 件の賞賛
返信