CSEc Module for storing secure Encrypted keys and secure boot support in S32K144 MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CSEc Module for storing secure Encrypted keys and secure boot support in S32K144 MCU

3,232 Views
mrajanna
Contributor V

I have gone through below document as well the source code but still I need more information.

http://www.nxp.com/docs/en/application-note/AN5401.pdf

I want to know below details:
a. For the first time how secure keys are loaded into Flash. 
b. 512KB Memory split in S32K144. Memory architecture. 
c. How secure boot is implemented.
d. Any presentation or pdf on CSEc module in S32K144.
e. How CAN messages can be authenticated using CSEc module.
f. After purchase of evaluation board, Would I get help to program secure encrypted keys and secure boot.

Tags (1)
0 Kudos
Reply
1 Reply

2,281 Views
liulei1
Contributor II

Hello, my problem is the same as yours. Have you solved it?

0 Kudos
Reply