CSEC ON 32K148

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CSEC ON 32K148

6,581 Views
hajianik
Senior Contributor I

Hi,

My target is S32K148.

I'm running the NXP project (Configure_parts_and_load_keys) with a little bit of modification:

This mode will change the MASTER_ECU_KEY_Value from blank(0xFFs) to zero,

Also will load zero in KEY_1 slot(key_id=4).

while it is successful in loading zeros in MASTER_ECU_KEY slot(key=1)

by comparing calculated M4,M5 to M4_OUT/M5_OUT however it fails with loading KEY_1 with the zero value.

uint32_t BLANK_KEY_VALUE[4] = {0xFFFFFFFF, 0xFFFFFFFF, 0xFFFFFFFF, 0xFFFFFFFF};

uint32_t ZERO_KEY_VALUE[4] = {0x00000000, 0x00000000, 0x00000000, 0x00000000};

//install zero values for Master_ECU_KEY

calculate_M1_to_M5(M1, M2, M3, M4, M5, BLANK_KEY_VALUE/*ZERO_KEY_VALUE*/,/*MASTER_ECU_KEY_VALUE_1*/ ZERO_KEY_VALUE, MASTER_ECU_KEY, MASTER_ECU_KEY, 1, 0); /* Calculate M1 to M5 in Software */

csec_error = LOAD_KEY(M4_out, M5_out, M1, M2, M3, MASTER_ECU_KEY); /* Load the key using SW calculated M1 to M3, and it returns M4 and M5 */

result = compare_results(M4, M4_out); /* Compare M4 generated by SW with the M4_out returned by CSEc */

 

/* Load KEY_1 */

calculate_M1_to_M5(M1, M2, M3, M4, M5, /*MASTER_ECU_KEY_VALUE*/ZERO_KEY_VALUE,/* KEY_1_VALUE*/ZERO_KEY_VALUE, MASTER_ECU_KEY, KEY_1, 1, 0); /* Calculate M1 to M5 in Software, Authorizing Key = Master ECU Key */

csec_error = LOAD_KEY(M4_out, M5_out, M1, M2, M3, KEY_1); /* Load the key using M1 to M3, returns M4 and M5 */

result = compare_results(M4, M4_out); /* Compare M4 generated by SW with the M4_out returned by CSEc */

Please tell me what I'm doing wrong.

Koorosh Hajiani

Tags (1)
0 Kudos
Reply
11 Replies

6,570 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I did quick test on my side and it works. The only thing I changed in default project Configure_parts_and_load_keys from AN5401 is CSEc_keys.h:

uint32_t MASTER_ECU_KEY_VALUE[4] = {0, 0, 0, 0};

uint32_t KEY_1_VALUE[4] = {0, 0, 0, 0};

No other changes.

Output of compare_results() function was 1 (success) in both cases.

Regards,

Lukas

 

0 Kudos
Reply

6,556 Views
hajianik
Senior Contributor I

Hi Lucas,

I followed your advise and it did not work.

I mean I still can not load KEY_1, NOW YOU JUST CHANGE THE NAME OF POINTER TO THE FUNCTION. THAT SHOIULD NOT MATTER.

I did what you did however the result is the same :

I can successfully load the ECU_MASTER_KEY_VALUE of zeros but it fails in loading KEY_1.

I used several boards to do this, the RESET_PARTS_TO_FACTORY_RESET does not work even with

ECU_MASTER_KEY_VALUE of zeros . so each time I need to do this on a new PCB.

This a mystery, here is the modified code based on your suggestion:

* CSEc_keys.h
 *
 *  Created on: Oct 19, 2016
 *      Author: B55457
 */

#ifndef CSEC_KEYS_H_
#define CSEC_KEYS_H_

uint32_t BLANK_KEY_VALUE[4] =   {0xFFFFFFFF, 0xFFFFFFFF, 0xFFFFFFFF, 0xFFFFFFFF}; //When key value is not written it is all FFs
//uint32_t MASTER_ECU_KEY_VALUE[4] = {0xD275F12C, 0xA863A7B5, 0xF933DF92, 0x6498FB4D}; //MASTER_ECU_KEY
//uint32_t MASTER_ECU_KEY_VALUE[4] =      {0x43414e44, 0x69566120, 0x4d535452, 0x204b4559}; //MASTER_ECU_KEY_GM
uint32_t MASTER_ECU_KEY_VALUE[4] = {0, 0, 0, 0};

uint32_t KEY_1_VALUE[4] = {0, 0, 0, 0};

uint32_t BOOT_MAC_KEY_VALUE[4] = {0x12340000, 0x00000000, 0x00000000, 0x00005678}; //BOOT_MAC_KEY
//uint32_t KEY_1_VALUE[4] =   {0x2FF8B03C, 0x5C540546, 0x5A9C94BD, 0x2D863279}; //KEY_1
uint32_t KEY_11_VALUE[4] =   {0x85852FF8, 0xE7860C89, 0xB3AB9D63, 0xB8D6288F}; //KEY_11
uint32_t RAM_KEY_VALUE[4] =   {0x68B674CB, 0x8198A250, 0x3A285100, 0xF4DDC40A}; //RAM_KEY
//uint32_t ZERO_KEY_VALUE[4] = {0x00000000, 0x00000000, 0x00000000, 0x00000000};
#endif /* CSEC_KEYS_H_ */

/* Load KEY_1 */

calculate_M1_to_M5(M1, M2, M3, M4, M5, MASTER_ECU_KEY_VALUE/*ZERO_KEY_VALUE*/, KEY_1_VALUE/*ZERO_KEY_VALUE*/, MASTER_ECU_KEY, KEY_1, 1, 0); /* Calculate M1 to M5 in Software, Authorizing Key = Master ECU Key */

csec_error = LOAD_KEY(M4_out, M5_out, M1, M2, M3, KEY_1); /* Load the key using M1 to M3, returns M4 and M5 */

result = compare_results(M4, M4_out); /* Compare M4 generated by SW with the M4_out returned by CSEc */

Thanks,

Koorosh Hajiani

Tags (1)
0 Kudos
Reply

6,542 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

attached are working projects.

Notes:

- it's necessary to execute both projects from RAM

- when resetting back to factory state, it's necessary to change the MASTER_ECU_KEY directly in DBG_AUTH function. It's hardcoded here for some reasons. The CSEc_keys.h file is not used here:

lukaszadrapa_0-1615293391028.png

- and I found small bug in startup code when creating new application project in S32DS 2.2 for S32K148. Not sure what kind of project you have but maybe for others - it's necessary to call SystemInit after stack initialization. Move it like this:

lukaszadrapa_1-1615293784604.png

 

Regards,

Lukas

 

0 Kudos
Reply

6,537 Views
hajianik
Senior Contributor I

Hi,

I was the culprit, I was messing around with calculate_M1_TO_M5 function for keys greater than or equal than KEY_1.

I DELETED MY CHANGES AND IT SEEMS TO BE WORKING.

sorry for wasting your time. just one more question :

For keys who reside on bank1(kbs=1) would these function work?

Thanks,

Koorosh

Tags (1)
0 Kudos
Reply

6,520 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Koorosh,

yes, no difference, it's the same for kbs=1.

Regards,

Lukas

 

0 Kudos
Reply

6,482 Views
hajianik
Senior Contributor I

Hi Lukas,

When updating a key, in addition to updating its value can we change its attributes?

 

Thanks,

Koorosh

 

0 Kudos
Reply

6,460 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Koorosh,

yes, the attributes can be changed when updating a key.

Regards,

Lukas

 

0 Kudos
Reply

6,469 Views
hajianik
Senior Contributor I

Hi Lukas,

which part numbers of S32K148 will support the GM_SHE (20 KEY SLOTS).

I have the S32K 148_EVAL BOARD that supports only 17 slots, on the production PCB same code supports 10 slots.

Thanks,

Koorosh

0 Kudos
Reply

6,459 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Koorosh,

if CSE is available, there are 20 Keys. If you can use only 10 keys then you have configured 10 keys by Program Partition command:

lukaszadrapa_0-1616056409066.png

Regards,

Lukas

 

0 Kudos
Reply

6,444 Views
hajianik
Senior Contributor I

Hi Lucas,

Thanks for your response.

well it clears it up that we have 20 slots and only 17 user key. then why the enum

csec_key_id_t goes passed key_17, all the way through key_21?

second part of my question:

It is the same code that's running both on the EVAL board and the production board.

On the eval board I can load key_1 to key_17 however on the production board the same code will load key slots from key_1 to key_10.

any attempt to load passed key_10 fails.(production part number:SC668037VMH/R) which would support 20 keys.

 

Thanks,

Kooosh

Tags (1)
0 Kudos
Reply

6,427 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Koorosh,

SC668037VMH/R is a custom part number and I can see there are some differences. Please ask your OEM for details. I'm not allowed to share details about custom devices.

Regards,

Lukas

 

0 Kudos
Reply