CSEC_BOOT_MAC update fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CSEC_BOOT_MAC update fail

2,051件の閲覧回数
wang_q4
Contributor I

Dear all,

When updating CSEC_BOOT_MAC, CSEC_DRV_LoadKey() returned an update failure. The return value of the failure is STATUS_SEC_KEY_UPDATE_ERROR.May I ask the reason for this failure to rest

PS: I used the auth key is master key.

0 件の賞賛
返信
2 返答(返信)

2,011件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I can't see reason for this. BOOT_MAC can be updated with knowledge of old value of BOOT_MAC or with knowledge of MASTER_ECU_KEY. Counter needs to be incremented appropriately. How do you calculate M1-M5 values? Are you sure that correct values are provided?

Regards,

Lukas

0 件の賞賛
返信

2,029件の閲覧回数
wang_q4
Contributor I

Add: using master key as the auth key, i can update other keys

0 件の賞賛
返信