CLKOUT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLKOUT

3,201 Views
liulei1
Contributor II

I want use CLKOUT,so,I config the SIM->CHIPCTL as:

PCC->PCCn[PCC_PORTD_INDEX] |= PCC_PCCn_CGC_MASK;
PORTD->PCR[14] |= 7<<8; 
SIM->CHIPCTL|=SIM_CHIPCTL_CLKOUTEN(1)|SIM_CHIPCTL_CLKOUTSEL(8)|SIM_CHIPCTL_CLKOUTDIV(1);

But I only saw a waveform of 128KHZ, no output SPLLDIV2_CLK

0 Kudos
Reply
2 Replies

3,045 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

Could you please tell me which MCU do you use?

 

I tested it on the S32K144.

My clock settings:

SPLL = 160MHz

SPLLDIV2 is divided by 4 = 40 MHz

My clkout init function:

void CLKOUT_init(void)
{
PCC->PCCn[PCC_PORTD_INDEX]=PCC_PCCn_CGC_MASK; //Enable clock for PORTD
PTD->PDDR |= 1<<14; //Port D14 is configured as output
PORTD->PCR[14] |= PORT_PCR_MUX(7); //Alternative 7, set pin as CLKOUT
SIM->CHIPCTL |= SIM_CHIPCTL_CLKOUTSEL(8); 
SIM->CHIPCTL |= SIM_CHIPCTL_CLKOUTDIV(0); //Output clock divide by 1
SIM->CHIPCTL |= SIM_CHIPCTL_CLKOUTEN(1); //Enable CLKOUT

}

After that, I can measure 40 MHz on the CLKOUT pin.

I hope it helps you.

Best Regards,

Diana

0 Kudos
Reply

3,045 Views
liulei1
Contributor II

I have found the problem, the S32K144 I used should be an early engineering sample, there are some bugs. I changed a piece of the latest development board, there is no problem.Thank you.

0 Kudos
Reply