CDD_Rm_S32k322

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CDD_Rm_S32k322

3,336件の閲覧回数
gadilinga
Contributor III

Hi team,                                                                                                                                                                                  for above subject I'm using  motor control application in SWC CDD RM. I'm Using in that many features is there  XBIC, XRDC, Pflash , semaphore and Virtual Wrappers, plz guide us for purpose of these feature in the Resources manager in CDD_RM SWC. actually in Motor controller application, in Reference manual much details not available so kind plz give me some input for my application how its use full to motor controller.

thank u  

0 件の賞賛
返信
7 返答(返信)

3,287件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you be more specific what you are looking for?

What SWC CDD RM stands for?

Could you post link to NXP product you are talking about? It is some motor control kit or?

Best regards,

Peter

0 件の賞賛
返信

3,276件の閲覧回数
gadilinga
Contributor III
Hi @petervlna,

thank u so much u r response Actually I'm Using S32K322 Customized Board, Based on the Reference of S32K344 Application Note 13767. here I need to Use CDD_RM for this Application so that In that CDD_RM So many Features will be there like XBIC, XRDC, Pflash , semaphore and Virtual Wrappers, how these Feature Useful to the S32K322 . what was the Purpose these feature for Motor controller Application. plz guide us for more explore regarding this Components. thank u
0 件の賞賛
返信

3,258件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

OK, but i still do not know what What SWC CDD RM stands for?

Is it some SW you are going to write or some general driver or?

Motor control applications are located at our web page:

https://www.nxp.com/applications/enabling-technologies/motor-control:MOTOR-CONTROL

Best regards,

Peter

 

0 件の賞賛
返信

3,240件の閲覧回数
gadilinga
Contributor III
Hi @petervlna,
thank u for reply CDD_RM(Resources manager),RM module provides a way to initialize and control the resource domains allocation and memory protection on the chip with the supported peripherals. Resource Management (RM) is critical for controlling access to shared hardware resources within the microcontroller. these are the HE resources XBIC, XRDC, Pflash , semaphore and Virtual Wrappers. thank u
0 件の賞賛
返信

3,224件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Ok, thank you for explanation.

I was confused by CDD which usually stands for complex device driver, which means its the autosar module your wrote yourself.

Regarding RM plugin, there is a doc folder where integration and user manual are located:

petervlna_0-1735890946884.pngpetervlna_0-1735890946884.png

Where the GUI and API is described in details.

On top of that there are multiple example SW included in folder example:

petervlna_1-1735891045280.pngpetervlna_1-1735891045280.png

Best regards,

Peter

0 件の賞賛
返信

3,215件の閲覧回数
gadilinga
Contributor III
Hi @PetercIna,
thank u for U r quick response, yeah I seen whatever u shared information But query is that in the Rm many features will be there there XBIC, XRDC, Pflash , semaphore and Virtual Wrappers, plz guide us for purpose of these feature in the Resources manager. for Motor Controller application. thank u
0 件の賞賛
返信

3,187件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Hmm, not sure what you really asking for.

The documentation regarding API is included as I have explained.

The documentation regarding the modules functionality is in reference manual.

See chapters for XBIC, XRDC, Pflash , semaphore and Virtual Wrappers.

I am really confused by whole this thread.

Do you need assistance with SW development?

Or do you need specific module functional explanation beyond the reference manual?

Also motor control application - you can use those or not, it depends on the application.

If you could formulate your question clearly and specifically I can answer it, but for general tutorial you can request trainings via NXP FAE/distributors or via online courses if there are such.

Best regards,

Peter

0 件の賞賛
返信